Does anyone have an update on the cases? Is it still mid June? And I understand that a Raspberry Pi 4 faceplate might be in the offering soon.??
Hi,
I purchased a ReComputer Case with an Odyssey middle April, so far I received nothing…
Recent Orders|Order #|Date|Ship To|Order Total|Status|Action|
|4000034169|4/21/20|nl.smart|$235.81|Confirmed| View Order|
Hi,
The case will be back in stock in around early-July. We will ship your parcel out once all the items are available. Hope you can understand!
Thanks for your reply.
Is it possible to receive my ReComputer Case without Aluminum Anodizing Process ?
It’s no problem for me, the aluminium don’t care about the rust 
It will be an original case, for sure.
Send me the ReComputer Case (without Aluminum Anodizing Process) with the Odyssey - X86J4105800 I purchased.
nl.smart.
Hi,
I purchased an Odyssey and the case April 17 (order #4000033739).
Do you guys have an estimate date of my order’s shipping?
Hi,
I purchased in April.
I received case and device today 
First I updated the bios
Enjoy.
[manjaro@manjaro ~]$ screenfetch
██████████████████ ████████ manjaro@manjaro
██████████████████ ████████ OS: Manjaro 20.0.3 Lysia
██████████████████ ████████ Kernel: x86_64 Linux 5.6.15-1-MANJARO
██████████████████ ████████ Uptime: 5m
████████ ████████ Packages: 1217
████████ ████████ ████████ Shell: bash 5.0.17
████████ ████████ ████████ Resolution: 1920x1080
████████ ████████ ████████ DE: KDE 5.70.0 / Plasma 5.18.5
████████ ████████ ████████ WM: KWin
████████ ████████ ████████ GTK Theme: Breath [GTK2/3]
████████ ████████ ████████ Icon Theme: breath2
████████ ████████ ████████ Disk: 79G / 85G (94%)
████████ ████████ ████████ CPU: Intel Celeron J4105 @ 4x 2.5GHz [46.0°C]
████████ ████████ ████████ GPU: Mesa Intel(R) UHD Graphics 600 (GLK 2)
RAM: 1579MiB / 7800MiB
[manjaro@manjaro ~]$ inxi -F
System: Host: manjaro Kernel: 5.6.15-1-MANJARO x86_64 bits: 64 Desktop: KDE Plasma 5.18.5
Distro: Manjaro Linux
Machine: Type: Desktop Mobo: SeeedStudio model: ODYSSEY-X86J4105 v: SD-BS-CJ41G-M-101-E 01/07/2020 14:03:11
serial: <root required> UEFI: American Megatrends v: SD-BS-CJ41G-M-101-E date: 01/07/2020
CPU: Topology: Quad Core model: Intel Celeron J4105 bits: 64 type: MCP L2 cache: 4096 KiB
Speed: 998 MHz min/max: 800/2500 MHz Core speeds (MHz): 1: 998 2: 995 3: 998 4: 999
Graphics: Device-1: Intel UHD Graphics 605 driver: i915 v: kernel
Display: x11 server: X.Org 1.20.8 driver: intel unloaded: modesetting resolution: 1920x1080~60Hz
OpenGL: renderer: Mesa Intel UHD Graphics 600 (GLK 2) v: 4.6 Mesa 20.0.7
Audio: Device-1: Intel driver: snd_hda_intel
Sound Server: ALSA v: k5.6.15-1-MANJARO
Network: Device-1: Intel driver: iwlwifi
IF: wlo2 state: down mac:
Device-2: Intel I211 Gigabit Network driver: igb
IF: enp2s0 state: up speed: 1000 Mbps duplex: full mac:
Device-3: Intel I211 Gigabit Network driver: igb
IF: enp3s0 state: down mac:
Drives: Local Storage: total: 103.94 GiB used: 72.86 GiB (70.1%)
ID-1: /dev/sda vendor: Hitachi model: HTS541080G9SA00 size: 74.53 GiB
ID-2: /dev/sdb type: USB vendor: Transcend model: JetFlash Transcend 32GB size: 29.41 GiB
Partition: ID-1: / size: 5.71 GiB used: 142.7 MiB (2.4%) fs: overlay source: ERR-102
Sensors: System Temperatures: cpu: 43.0 C mobo: N/A
Fan Speeds (RPM): N/A
Info: Processes: 217 Uptime: 6m Memory: 7.62 GiB used: 927.3 MiB (11.9%) Shell: bash inxi: 3.0.37
[manjaro@manjaro ~]$ date -u
Mon 15 Jun 18:19:24 UTC 2020
[manjaro@manjaro ~]$
That’s great. I ordered 4/6. And then later updated to two cases. Got the cpu awhile back, but no case. I’m hoping I can put the little guy in a case soon.
Did you get any tracking info?
Yes, they provided a dhl tracking number.
So far the device is working well.
Good news… Just got a blanket email stating that they are caught up and I should get an email shortly about the shipment. Cool.
Happy to know, I hope you’ll appreciate the device.
I got my cases in last week. That’s a really nice case. Power button a little hard to get in place but after some effort… It works fine.