reCamera: Build Vision AI Platform for Anywhere!

Here is my review of the AI camera recamera from Seeed Studio.

I was very excited about this camera. Within 30 minutes of unboxing I had finished by first program. The camera comes with the Linux operating system and node-red already installed with extra nodes to support the camera.

Compared to the M5Stack Unit V2 M12 or Unit V2, recamera has much more memory - my camera has 64GB compared to the 128MB in the V2 cameras. The recamera’s processors is also much more powerful and can zip along doing YOLO11 on object recognition over 80 classes at 30 frames a sec.

recamera has its downsides is that the recamera is much bigger than the Unit V2 and harder to install on small Lego model such as Robots. It also uses more power and it is very easy to lose your uSD card inside the recamera’s case. But its biggest downside is the way Seeed Studio implemented node-red. This will be explored in the next video.
Youtube: channel: dsrc12

1 Like