Hi guys, I am new here:
I would like to know if anybody can help me with this. I need to power a readiymate with a wind up crank… something like those wind up radios. I was thinking of also using a lipo pro to capture the charge from the generator (dynamo) but I am not sure if that will produce enough current. How do I check that? As anybody used a wind up crank on the lipo before? How would I connect it? And what battery shall I buy?
Please help asapppp!
Thanks
or maybe someone can advise me if it will work with a normal arduino just to start off with.
at the moment i am using this wind up generator here, for specifics: dgyingyi.en.alibaba.com/product/ … rator.html
Hi,the input of lipo rider is : DC: Vmin 4.8v Vmax 6.5v Imin 400mA Imax 600mA
So, you need a rectifier units , and confirm that your output voltage of generator(the current out of generator is AC, so current should be rectified) less than 6.5v and more than 4.8v.
then , you can connect the output of generator to input of lipo rider.And you can use a 3.7v lithium battery.
But your generator has three wires , we don’t have the datasheet . So you might do it refer to previous parameters.
Hi Jacket Chen,
this really makes things much more clear! Thanks so much for your reply! 
Now, I have another generator that I found in a torch which is connected to a bridge rectifier called DB107, I was thinking: do you reckon that would supply the right amount of power?
Specs here: diodes.com/_files/products_i … 211_R5.pdf
Hello again,
I just tried checking with a multimeter and that rectifier is exactly what you meant!
it’s outputting DC!
The problem is that it easily goes over 6.5V which will blow the Lipo Rider, right?
Could you advice me on a bridge rectifier which would output only the required current/voltage?
Thanks!
Hi , the outputting DC voltage could not more than 6.5v.
you can choose a rectifier that can turn your outputting DC voltage to 5v.And if the outputting DC current is more than 600mA, you just add a proper resistor that can decrease your current.
hi there,
could you maybe advise me on a rectifier that does that?
please! thanks a lot!
First , you can use a rectifier diode(IN4001), turn AC to DC , and then use a DCDC module(LM2595,http://www.ti.com/product/lm2595), so you can get a 5v voltage.