Read/write devNonce value

Hi,
I getting known problem with "devNonce " while joining with LoRa-E5 module (LoraWAN 1.0.2).

I wonder if it is possible to read/write “devNonce” value from LoRa-E5 module?

LoRa-E5 module settings was changed from LoraWAN 1.0.2 to LoraWAN 1.0.3, but the problem with “devNonce” remains.

Since I minimize Join events (Join event is calling only at device power on), module connection to gateway ant further works better. Minimizing Join events to minimum is also recommendation for using LoraWAN.

Or command FDEFAULT reset “devNonce”?