RE: The HDMI Cape for the BBG

Hello,

Is the HDMI Cape for the BBG de funct?

Seth

P.S. If so and if the new firmware is not working, please reply. I was trying to figure out this info. for another individual.

This only works with Linux kernel version 4.4. With the new firmware, you also need to install the Linux kernel 4.4. 4,4 is also the kernel of the LTS version.

1 Like

Hello Sir,

Thank you for your reply. Kernel 4.4.x only. Got it.

Seth

hello @Baozhu , can you please post the link to a BB OS image that works with the HDMI cape?
If possible, I need a flasher image to boot from eMMC.
I want to use the HDMI cape with a BBGW, is it compatible?
THanks