I would appreciate a slight redesign of the re_case that would allow GPIO access for the ODYSSEY-X86J4105. By that I mean being able to plug into the GPIOs (both for the onboard microcontroller and PC pins) without having to remove the top of the case. For example similar side panels to how the USB/HDMI ports are accessed. Cables randomly dangling from the top is very frustrating (and in my opinion really defeats the purpose of this machine).