Raspberry 4b with ReSpeaker 6-Mic don't work

Hi!

When i install seeed-voicecard by

sudo apt-get update
sudo apt-get upgrade
git clone GitHub - respeaker/seeed-voicecard: 2 Mic Hat, 4 Mic Array, 6-Mic Circular Array Kit, and 4-Mic Linear Array Kit for Raspberry Pi
cd seeed-voicecard
sudo ./install.sh
sudo reboot

there are some problems that:

so,i use

rm -R seeed-voicecard/
git clone GitHub - HinTak/seeed-voicecard: This is an enhancement fork with the explicit aim of supporting current shipping Raspbian/Ubuntu kernels without requiring downgrading. Please donate at https://hintak.github.io/ if it works for you. Use vX.Y branch for kernel version vX.Y
cd seeed-voicecard
sudo ./install.sh

the seeed-voicecard can be successful install,but when i check the sound card ,there have another problem:

pi@raspberrypi:~ $ arecord -L
null
Discard all samples (playback) or generate zero samples (capture)
jack
JACK Audio Connection Kit
pulse
PulseAudio Sound Server
default
ac108
dmixer
ac101
usbstream:CARD=b1
bcm2835 HDMI 1
USB Stream Output
usbstream:CARD=Headphones
bcm2835 Headphones
USB Stream Output

pi@raspberrypi:~ $ aplay -L
null
Discard all samples (playback) or generate zero samples (capture)
jack
JACK Audio Connection Kit
pulse
PulseAudio Sound Server
default
ac108
dmixer
ac101
sysdefault:CARD=b1
bcm2835 HDMI 1, bcm2835 HDMI 1
Default Audio Device
dmix:CARD=b1,DEV=0
bcm2835 HDMI 1, bcm2835 HDMI 1
Direct sample mixing device
dsnoop:CARD=b1,DEV=0
bcm2835 HDMI 1, bcm2835 HDMI 1
Direct sample snooping device
hw:CARD=b1,DEV=0
bcm2835 HDMI 1, bcm2835 HDMI 1
Direct hardware device without any conversions
plughw:CARD=b1,DEV=0
bcm2835 HDMI 1, bcm2835 HDMI 1
Hardware device with all software conversions
usbstream:CARD=b1
bcm2835 HDMI 1
USB Stream Output
sysdefault:CARD=Headphones
bcm2835 Headphones, bcm2835 Headphones
Default Audio Device
dmix:CARD=Headphones,DEV=0
bcm2835 Headphones, bcm2835 Headphones
Direct sample mixing device
dsnoop:CARD=Headphones,DEV=0
bcm2835 Headphones, bcm2835 Headphones
Direct sample snooping device
hw:CARD=Headphones,DEV=0
bcm2835 Headphones, bcm2835 Headphones
Direct hardware device without any conversions
plughw:CARD=Headphones,DEV=0
bcm2835 Headphones, bcm2835 Headphones
Hardware device with all software conversions
usbstream:CARD=Headphones
bcm2835 Headphones
USB Stream Output

Please try again

sudo apt-get update
sudo apt-get upgrade
git clone https://github.com/respeaker/seeed-voicecard.git
cd seeed-voicecard
sudo ./install.sh  --compat-kernel
sudo reboot

Hey Baozhu!

I’ve tried doing the install with the compat kernel, but unfortunately it still does not register the soundcard upon reboot.

I had been using the respeaker 6 Mic for months with no problem. I had to reflash my SD cards last week, and upon clean soundcard install it wouldn’t work without the compat-kernel. I tried the compat kernel install and it worked for a few days. But this morning, I restarted the device and the sound card no longer appears to exist.

I’ve tried the HinTak version and still no luck either.

I have bought 4 of these arrays and now none of them are usable. Please help! We were hoping to use these devices in field research which was due to start imminently!

Good luck with that ! According at messages in forum since a while it looks like SeeedStudio doesn’t care about updating these drivers to keep Respeaker products working !! They don’t even give a status about it and if they are working on it :frowning:
I have myself same problem with some Raspberry Pi that I had to reinstall and now can no more Respeaker hats installed on them :rage:

Im having exactly the same issue with a pi 4b and a respeaker 4.
Would be great if seeed could update it to work properly with the latest versions