Rainbowduino V2.0 with FTDI Friend Chip

Hi,

I’m trying to get my LED 8x8 Matrix working with a Rainbowduino V2.0 that is connected to a FTDI Friend by adafruit. I’ve put the wires the following way:

Rainbowduino - FTDI
RX - TX
TX - RX
VCC - VCC
DTR - RTS
GND - GND

I’ve selected Arduino Duemilanove w/ AT Mega 328.

I’ve downloaded the Rainbowduino library right here:
seeedstudio.com/wiki/images/ … ino1.0.zip

When I try to upload a simple sketch, for example shapes, the FTDI blinks correctly showing that it is uploading but I get nothing in the LED matrix. And my LED matrix is working because I test it in other board.

Is there a different library only for Rainbowduino v2.0? Sketches from rainbowduino v3.0 won’t work with my v2.0? Am missing any connection?

Thanks!

bump

It looks like Rainbowduino V2 is not compatible with the library available in the wiki. It’s only for V3.0. I spent good 3 hours trying to figure out why!
Can someone make the old version of the library available?

bump! grr!