Rainbowduino (LED Cube Matrix Question)

Thanks for the information.

Was a bit confused at what the schematic was for, but I am assuming it’s for the chasis they built for the cube that you put the LED’s into, and then tie into the PCB?

I’m guessing it’s just a matter of tying the common anodes of my cube into the inputs of the 8 npn transistor array they have built into the board, and then putting each individual column’s cathode into the 8 different RGB inputs they have.

The only thing i’m curious about at this point is whether or not I am going to be able to pull off a 5x5x5 cube because of the 24 output pins (8 X RGB) and i’d technically need 25, plus 5 for the common anodes of the 5 rows in the cube.