Rainbowdiuno

I have a brand new rainbowduino V3.0b. Out of the box I plugged it into my SEED LED matrix as I got the impression it had a demo program on it. All I get is a single red LED lit. If I try it with my LED cube which works fine on my rainbowduino V2 it does nothing. When I try to upload scetches from the wiki I get the following error: In file included from Cube1.cpp:7:
C:\Program Files (x86)\arduino-1.0\libraries\rainbowduino/Rainbowduino.h:33:22: error: WProgram.h: No such file or directory

Any assistance you could give would be greatly appreciated, I was trying to get the cube running for a Makerspace demo tomorrow )-:

Cheers,

Scott.

If anyone has any suggestions on this it would be greatly appreciated. I really need to have this up and running in about 12 hours time (-:

I think that problem is with arduino software v1.0.
I’ve just got my Stalker and had the same issue.
Sources at Wiki are not adapted to the latest 1.0 version. Try <= 0023 version.
Hope it helps!

Thanks Ursus,

You were spot on, I’m now up & running (-:

Cheers,

Scott.