Hi,
I can’t understand why the preassembled rainbowcube I have does not follow the coordinates rules as detailed into the wiki: If I use the cube1 example the three led I have on are not the same which should be; I have checked the cube using a testing code in order to put on every led of the matrix in sequence and surprisengly I have that the led sequence is not the one predicted but e.g. the coordinates x,y,z (2,2,0) is at (2,2,3). I have checked all the solders and I have found two shorted pins on a led and a missing solder but nothing more, now the cube is made as detailed into the assembly instructions. Any idea about that? Anybody experienced the same issue?
Wolf