Rainbow Cube problem

I have an issue with my Rainbow cube, One LED will not light up it’s green colour, and when I switch LEDs on and off with CubeXControl, it turns on multiple LEDs at the same time for some locations.

I know the LED is good, as it will light up all colours if I power it directly. I am assuming I have messed up the jumpers, or have missed a solder joint somewhere.

Is there a circuit schematic somewhere? I think I need one to track the problem with my multimeter.

Or any other suggestions?

Thanks
Duncan

Power runs up the riser from the base and is tied into the appropriate level via a jumper. The cube is divided into 8 sections since it is really just a remapping of 8x8 rainboduino to 4x4x4. You only connect one jumper on each riser and only one to each level on each side for a total of 8 jumpers soldered. If you connect more than one on a specific riser then all the LEDs on each of those levels (on that side) will light up at the same time.