RA4M1: huge noise in ADC values

I tested the ADC in the RA4M1 module and found that there is a huge amount of noise in the values. This is my test circuit:


This is the test software:

//  Seeed XIAO RA4M1 ADC Test
//  Michael Koch, September 2024

double x, mean, sigma;
double sum_x, sum_xx;
int n;

// the setup function runs once when you press reset or power the board
void setup()
{  
  analogReadResolution(12); 

  Serial.begin(115200);
  while (!Serial)
    delay(10);  
}

// the loop function runs over and over again forever
void loop()
{
  n = 10000;
  sum_x = 0;
  sum_xx = 0;
  for(int i = 0; i < n; i++)
  {
    x = (double)analogRead(A1);
    sum_x += x;
    sum_xx += x*x;
  }

  mean = sum_x / n;
  sigma = (sum_xx - n * mean * mean) / n;
   
  Serial.print("Mean: ");
  Serial.print(mean);
  Serial.print("   Sigma: ");
  Serial.print(sigma);
  Serial.println();
  delay(500);
}

The mean value is as expected, but there is a standard deviation of about 135.
The same software with a SAMD21 module has a standard deviation of about 4 (in the same test circuit).
Why does the RA4M1 have more noise by a factor 30? The ADC is almost unusable.

I did already try to use an external reference instead of the 3.3V reference (after removing R5 from the module) but it didn’t help much.

Michael

I forgot the square root in the formula for the standard deviation:
sigma = sqrt((sum_xx - n * mean * mean) / n);
But the problem remains the same: RA4M1 has much more noise than SAMD21 in the ADC values.

Updated test software with more statistic values:

//  Seeed XIAO RA4M1 ADC Test
//  Michael Koch, September 2024

double x, mean, sigma;
double sum_x, sum_xx;
double minimum, maximum;
int n;

// the setup function runs once when you press reset or power the board
void setup()
{  
  analogReadResolution(12); 

  Serial.begin(115200);
  while (!Serial)
    delay(10);  
}

// the loop function runs over and over again forever
void loop()
{
  n = 10000;
  minimum = 65535;
  maximum = 0;
  sum_x = 0;
  sum_xx = 0;
  for(int i = 0; i < n; i++)
  {
    x = (double)analogRead(A1);
    if (x < minimum) minimum = x;
    if (x > maximum) maximum = x;
    sum_x += x;
    sum_xx += x*x;
  }

  mean = sum_x / n;
  sigma = sqrt((sum_xx - n * mean * mean) / n);
   
  Serial.print("Mean: ");
  Serial.print(mean);
  Serial.print("   Sigma: ");
  Serial.print(sigma);
  Serial.print("   Minimum: ");
  Serial.print(minimum);
  Serial.print("   Maximum: ");
  Serial.print(maximum);
  Serial.print("   Maximum-Minimum: ");
  Serial.print(maximum - minimum);
  Serial.print("   Mean-Minimum: ");
  Serial.print(mean - minimum);
  Serial.print("   Maximum-Mean: ");
  Serial.print(maximum - mean);
  Serial.println();
  delay(500);
}

Hi,

Thank you for your detailed records. Our engineers are currently investigating this issue.

Hi,
We found that the problem was that the noise of the power supply to the ADC was too large. We changed the R4 from 0Ω to 15Ω, and the variance after repair is about 1~3. We will release the optimized version v1.01 soon.

When I order a new module now, will it have the 15R resistor? I saw that it has never been changed th the schematic diagram.