Hello,
I was wondering if the Arduino BLE library is compatible with the SEEED XIAO ESP32S3. If not, are there any libraries that are?
Also, is there a board like the SEEED XIAO ESP32S3, but smaller? (Preferably 0.5 inches in width)
Any help would be greatly appreciated. Thank you.
make sure you have your arduino IDE set up with XIAO ESP32S3 as the selected board… just not the generic ESP32 development board and use the BLE sketches from that library
The chip will uses slightly different command structure
I do not know of anything smaller
Hi there,
Yes, Without the USB-C on board.
HTH
GL
PJ
Thank you both for your responses. @PJ_Glasso are you saying there is a board like the XAIO ESP32S3 but smaller, without a USB-C port? If so, would you be able to provide a link?
Hi there,
Not exactly like a xiao & No…I have only seen a prototype. Something close to it on the net here.
the beetle is one. and Paul Made this on Hakaday…
HTH
GL

PJ