Hi All!
Just a quick question, has anyone used the RB-See-98 water flow sensor as a speedometer for model boats? If so, how would you do the calculations from flow to speed?
Thanks, Ed
Hi All!
Just a quick question, has anyone used the RB-See-98 water flow sensor as a speedometer for model boats? If so, how would you do the calculations from flow to speed?
Thanks, Ed
You can probably only get an estimated velocity.
Since its pulse rate is based on the volume of water that flows throught it, and the section is constant, you can see that pulse rate is proportional to the speed.
To determine the proportionality constant you can try a simple experiment:
The difference between the two levels, divided by the number of pulses - 1, is the “space per pulse” = K .
So the speed will be “pulses * K / time”.
I said it’s not accurate because at very low (or very high) speeds, water dynamics might alter assumptions. For example, at very high speed the extra resistance offered by the sensor could make water “prefer” another way, so reducing the actual flow throught the sensor and making you measure a lower velocity. The best way to handle these situations could be to actually measure the number of pulses generated while traveling the same distance at various speeds.
Thank you ndk.clanbo!
I was just wondering a few things. Does the sensor put out 1 pulse per revolution or more? For if you know the diameter of the wheel and the number of pulses per revolution, could you not just a calculation based upon pulses per minute? Thanks, Ed
Sorry, I don’t have flow sensor (yet… maybe in next order, hope to add it to some current sensors as in wish)…
The most probable thing is that it does only one or two pulses per round (isn’t it on the wiki page? no… just checked, but you can do some math:
So, given the flow into the sensor is equal to the flow around the boat (strong assumption!), for every pulse it advanced about 1,2cm.
Check actual figures 'cause I’m quite tired and I could have done something wrong!