jensma
August 28, 2013, 8:04pm
1
Hello guys!
I’m not sure which version of the firmware I have. The bootloader says 3.26D while the bootscreen says 4.21. The DSI does have a micro SD slot.
I do want to upgrade the device. Can anyone tell me what would the correct benf version would be?
Thanks in advance!
Cheers,
jensma
Edit: Nevermind about the version, this thread helped me out: viewtopic.php?f=22&t=4632
Still wondering about a suitable benf firmware tough
dso.218
September 2, 2013, 1:16pm
2
Same as mine, doesn’t seem to be any way to upgrade to the benf firmware at the moment.
See this thread …
http://www.seeedstudio.com/forum/viewtopic.php?f=22&t=3195&start=100
d0m1n1k
September 5, 2013, 2:15pm
3
Same here.
The seller wrote “DSO NANO Hardware 1.6 + Paul’s Firmware 1.5”.
What is Paul’s Firmware 1.5? At web I found it’s a third party firmware? Where can I get it? Or is Ver4.21 already this “third party” firmware? If so, where can I get the original firmware?
Actually I decided to use the Benf Firmware. But it’s not possible at the moment, as I read in different threads here. . I suppose I have to sent it back.
d0m1n1k:
Same here.
The seller wrote “DSO NANO Hardware 1.6 + Paul’s Firmware 1.5”.
What is Paul’s Firmware 1.5? At web I found it’s a third party firmware? Where can I get it? Or is Ver4.21 already this “third party” firmware? If so, where can I get the original firmware?
Actually I decided to use the Benf Firmware. But it’s not possible at the moment, as I read in different threads here. . I suppose I have to sent it back.
Here, minidso.com/bbs/read.php?tid=408 DS0201 Firmware Update
d0m1n1k
September 21, 2013, 5:16am
5
I don’t see any “Paul’s Firmware” at that site? I already tried out FW Ver4.22, but nothing changed.