Thanks for sharing your information with us.
The square wave is the correct input for circuit frequency compensation. This is because perfect square edges of a square wave requires an infinite number of odd harmonics. You adjust for no overshoot and no undershoot of the leading edge. Adjust as close to a square leading edge as possible.
Attached is a screen capture of the pictures found at:
seeedstudio.com/blog/2009/12 … -dso-nano/
Can you remember if the caps are under the number “6” in the picture?
Thanks