When opening my DSO201 V2.4, I found two variable capacitors C2A and C7A with 10 and 30 pF respectively. What is the purpose of these elements?
Greets,
Reini
When opening my DSO201 V2.4, I found two variable capacitors C2A and C7A with 10 and 30 pF respectively. What is the purpose of these elements?
Greets,
Reini
These are used to compensations for better waveforms.
please can you more explain how to calibrate these caps? (reference frequency, voltage …)
ohh,it seems hard to explain the reason,l 'd like to say my own opinion for your ref:
Maybe you could describe the location of the adjustable caps on the unit. After looking at the dissassembly pictures provided by others, I don’t see them.
Thanks
take the back cover of DSO apart, you could see two adjustable caps near CN1(proble connector), that is C2A and C7A
there is also a easy way to calibrate C2A and C7A,just input a square wave signal instead of sine wave , for C2A,with p-p 0.5 v and any frequency you like,and adjust V/div to 0.1V/div, then ,ajust the C2A to make sure the wave in your DSO is the same as the signal input ;for C7a , ,with p-p 3 v and any frequency ,and adjust V/div to 1V/div,ajust the C7A to make sure the wave in your DSO is the same as the signal input .
in this way,you do not need to sinewave which may diffcult to get , just use square wave signal instead.
Thank you for your good description.
I’ll try this next time I reopen my Nano.
And I’ll shoot a photo of the Caps location.

there is also a easy way to calibrate C2A and C7A,just input a square wave signal instead of sine wave , for C2A,with p-p 0.5 v and any frequency you like,and adjust V/div to 0.1V/div, then ,ajust the C2A to make sure the wave in your DSO is the same as the signal input ;for C7a , ,with p-p 3 v and any frequency
Thanks for sharing your information with us.
The square wave is the correct input for circuit frequency compensation. This is because perfect square edges of a square wave requires an infinite number of odd harmonics. You adjust for no overshoot and no undershoot of the leading edge. Adjust as close to a square leading edge as possible.
Attached is a screen capture of the pictures found at:
seeedstudio.com/blog/2009/12 … -dso-nano/
Can you remember if the caps are under the number “6” in the picture?
Thanks
When opening my DSO201 V2.4, I found two variable capacitors C2A and C7A with 10 and 30 pF respectively.
It would be good if you and others in this post would specify which circuit board you have. Mine is DSO201V1.3A and it has no adjustable capacitors. Instead it has fixed capacitors as shown in the linked pictures. Perhaps mine is newer or older and they only used fixed factory value caps. Perhaps ESP can explain who does and who doesn’t have trimmers.
These pictures have high resolution and can be made large enough to read the surface mount component labeling. Imgxxx41.jpg shows the caps.
I’m having trouble adjusting C2A - I input 2 KHz 0.5V square wave, set nano to 0.1V/div, but the wave is very low passed, and adjusting C2A has no noticeable difference.
I’m wondering about the possibility of replacing the TL082 opamp with a faster one 
At the following link are pictures of the V2 Nano circuit board. You can readily find the adjustable capacitors in these pictures.