Hello,
I am writing to hear if any of you have a solution to the problems i am encountering with my Wifi Shield V1.1 (seeedstudio.com/wiki/Wifi_Shield_V1.1).
There are two different problems;
The first problem i am encountering whenever i try to run any of the example programs. They connect well to the iPhone-hotspot, but after 20-30 seconds it will disconnect. Every single time. 20-30 seconds of being online, and then boom, disconnected, and have to restart the program and the cycle.
The other problem came when i tried solving the first. I read that i could try updating the firmware on the board by using the update tool. It went ok(ish) but didn’t say firmware update succesful. Now i am on 4.4.1 (i think) firmware, and this is even worse than before. I tried hard resetting like in this guide (seeedstudio.com/wiki/Wifly_1 … leshooting), but it didn’t work. I just got the error code “web_app not found”.
Does anybody have a possible solution to this problem?
Thanks in advance,
Anders