I am having problems getting a M.2 2280 1GB SSD to work with E10-1. I already have a reTerminal and it works. I tried to use the instructions on the wiki ( reTerminal E10-1 - Seeed Wiki ) but these seemed to be incorrect and incomplete.
The example shown for the Hard Drive Expansion only shows that the internal eMMC drive is available and that is what I get. The command "sudo dd if=/dev/sda3 of=/dev/null bs=512k count=500 " Fails.
Please advice how to correct this. Please also include complete instructions to install a M.2 2280 SSD including all procedures from detecting the SSD to partitioning, formatting and mounting the SSD.
Please include similar instructions of a Mini PCLi SSD. I also attempted this but it failed.