Problems with GPRS shield - HTTP request

Hi!!
I have a problem with your GPRS SHIELD.

I try to do an HTTP request like this

AT+CSQ AT+CGATT? AT+SAPBR=3,1,"CONTYPE","GPRS" AT+SAPBR=3,1,"APN","mobile.vodafone.it" AT+SAPBR=1,1 AT+HTTPINIT AT+HTTPPARA="URL","nic.ing.unimo.it/arduino/" AT+HTTPACTION=0 AT+HTTPREAD
This instructions work perfectly but only one time… If I want to do another HTTP request like this I have to switch off the shield and, after turn on, do the same instructions another time. I have the same problem when i load on arduino this sketch (with the same parameters of the AT commands upside), that is present in the page about gprs shield, and i try to do more than one HTTP request…
seeedstudio.com/wiki/GPRS_Sh … e_Examples
The return of the HTTP request is often 408 (request timeout), sometimes nothing…
Can you give me some help?

You could try to use “AT+HTTPTERM” command to terminate HTTP service after HTTP request. More informations, please see the SIM900 AT command.

Hope it will help you.

Deray