Hi there,
I am working on a project where I am using the DPS310 to get altitude measurements. I want to connect the sensor to a Raspberry Pi but the I2C and SPI pins are not available. This is the reason why I connected the Grove connector from the DPS310 to a MCP3008 ADC which is connected to the Raspberry Pi. Is this possible to get the pressure/altitude from the analog signal output of the Grove connector?