Problem with seeed xiao ble nrf52840 and Arduino example

I have very big problem ))

My board Seeed XIAO BLE nRF52840 and

I opened project “Transmit_Recive” in Arduino IDE

when compiling it gives the following errors

Please, Help me!!!


2024_09_05_07_23_41_Transmit_Receive_Arduino_IDE_2.3.2

i think sensecap mate is a different module

Hi @Vovanxp ,
That sample sketch is included in the “Bluetooth examples for Wio Tracker 1110 Board” library.
This is for the Wio Tracker 1110 Dev Board, so it would not work with the XIAO nRF52840.