Problem with battery LED

Hi!

I’ve just received my quad and after playing around a few days, I’m thinking that it is a really nice tool and exactly fits my needs for playing with microcontrolers.

sys:1.52
app:2.53
hw: 2.7

But I’m having a small problem and it is an annoying one:
The red battery led is always on and it drains my battery without using the quad.

this means:
if power switch is OFF and usb-cable is not connected: red led is ON
if power switch is ON and usb-cable is not connected: red led is ON
if power switch is OFF and usb-cable is connected: red led is OFF
if power switch is ON and usb-cable is connected: red led is ON but dimmed

I think that this behavior is inverted to what it normally should do?

I’ve also tried other firmwares but no change.

Any suggestions?

Check out this thread.

viewtopic.php?f=26&t=4412

These indicate the battery charger IC may be faulty. You might want to consider getting a warranty replacement if it is new.

thanx for the info, haven’t found that thread through search, but it is exactly what was wrong.

ordered some LTC4054ES5-4.2, desoldered U14 (btw there was just a chip with un8hx, no ltc4045)
soldered the new one on the board and now everything seems to work fine.