Problem installing FreeNAS on eMMC Storage (read only file system, operation not permitted) Odyssey ReComputer

Yes I’ve enable CSM.
The file system on micsd0boot0 and mmcsd0boot0 are read-only and I assume that these are just the partitions of the SD Card I am using or the eMMC.
Or can I Plug the Odyssey in another computer and wipe the SD card as an external drive? Ist there a flash mode other than the boot mode on the odyssey?