I received my pre build rainbowduino today. Got everything up and running but 4 LEDs do have som glitches (the blue color wont work unless some pressure is made at the board). As mentioned this does only affect the blue color and the leds:
Z=2 Y=0 X=2
z=2 Y=0 X=0
Z=2 Y=2 Y=2
Z=2 Y=2 X=0
Where should I seek on the construction to find the fault? (I guess I could spend some time on the schematic to figure this out but since it was pre assebled Im to dissapointed that it is some problem at this moment )
What your mean push the bottom pcb in two of its corners? It mean Blue color can show up?If can provide a picture is better.
And Led has 4pin, just jump any wire for one pin to supply power(3.3v), check the LED work find.Jump from other LED is a easy way to supply 3.3V power.
Yes the 4 LEDs do work properly. If i apply some pressure on the corners (will send pictures in a few hours when I get home) the 4 LEDs work as they should so it seems that there is some glitches on the cube since they will work If I apply pressure on the right spot…
Sry havnt had time to send any pictures :S But last night I had my solderstation fired up dore some other projects and I thought that ill try to fix this.
The problem was a few starved solder joints in the led matrix ends so now everything seems to work!