Power jack size for Rainbowduino v3.0

Hello,

I ordered a Rainbowduino a couple of days ago and look forward to using it!

I searched the discussion forum for the power jack size on the Rainbowduino 3.0 and could not find an answer. I could only find the manual for the v1.2 Rainbowduino, which does not have a power jack. Can you provide the power jack size? Also, if you have a v3.0 manual, where can I find that?

Thank you,
Tom Hammond

How about the wiki:http://www.seeedstudio.com/wiki/Rainbowduino_v3.0?

Sorry, but the link to v3.0 information wiki does not indicate the size of the power jack. Do you know where I can find this information?

Hey the style of this connector is DC-005. and the inside diameter is 2.1 mm, the outside diameter is 5.5 mm. Maybe that would be helpful to you .