I’m using
sys v1.31
app v2.30
changing the volts per division will cause a change to the input stage, causing the signal to be distorted, I suggest there be a separate option to adjust zoom level (call it “adjust division size”)
all cursors, including the trigger threshold, currently stay where they are on the screen when you change the horizontal or vertical scaling. I’d rather they re-adjust their location according to the current scaling
the selected cursor should blink, that’d be nice
the option that is currently selected blinks, which is good, but when I scroll through options fast, I often don’t know what is currently selected during the blinking. So I suggest that the colour always go inverted when a new option is selected, I mean instantly instead of just using the blink timer. This would indicate which option is selected even if I’m scrolling really fast