Hi,
I’m trying to use Basler acA2440-20gc GIGE camera on reServer Industrial J4012 with PoE.
With frame size set to ~ 600x600 I can achieve at least 60FPS, but whenever I increase frame size (e.q. to 2000x2000) even 1FPS is too much and the camera disconnects.
The camera works properly on another Jetson device (Xavier). It also has no problems working on my vanilla laptop. MTU on the interface is set to 9000.
Driver for the Xavier is:
driver: igb
version: 5.10.120-tegra
whilst Orin has:
driver: lan743x
version: 5.10.104-tegra
Do you have any suggestions how can I diagnose this issue?
Thank you for all suggestions.
Hi there,
Curious to know Do you have any other device(s) connected to the other POE ports?
Are they by chance lower speed?
ie. 10/100?
In your other scenarios are they connected the same way “Hardware wise”?
9000 is that a JUMBO packet? setting on the NIC?
HTH
GL
PJ
What LED is lit when you plug the camera into the LAN ports on BACK?
Thanks for the reply,
Camera is the only device connected through POE. Both yellow and green LEDs are lit.
I think I have found the reason of camera failures.
The camera works properly when powered externally (i.e. not through PoE). It has power consumption ~ 3.3 W. Do you know if there’s any chance we can make it work with PoE?