Im having a hard time figuring out what the pins on the on the Xbee Shield v1.1 are corresponding to on the Xbee. Im refering to the both the male and female pins in the picture below. I tried several mails to support, but they just dont seem to understand my fairly simple question. Could someone help me? For ease of explanation, lets say that the left pin in the picture below is pin 1
Im not asking how to place it on the board, but what both the 1x8 male and the 2x8 (mine only has the one on the left) corresponds to on the Xbee. Which pin is the 5v, the Tx, the Rx etc.?