Hi everyone, I’m creating my first IoT project and I chose the Photon as my platform to develop the prototype.
I’m working with GROVE sensors and with a Particle Photon Base Shield.
One of my sensors is the Grove - Temperature&Humidity Sensor Pro(AM2302).
I readed the wiki section: 
<LINK_TEXT text=“http://wiki.seeedstudio.com/Grove-Tempe … Sensor_Pro”>http://wiki.seeedstudio.com/Grove-Temperature_and_Humidity_Sensor_Pro</LINK_TEXT>
And it says: Signal pin mode: digital. Also, below (In the Arduino section) you can read too:
“Step 1. Connect Grove - Temperature&Humidity Sensor Pro to port D2 of Grove-Base Shield.”
So I thought it was a digital sensor; but in the bag of the sensor there is a sheet of characteristics and it says that it’s an analog sensor.
so … ¿Where should I connect the sensor? A digital interface or an analogic one?
Thanks a lot.
Hi:
AM2302 is a digital sensor. It should be connected to the digital interface.
It includes a capacitive moisture sensing element and a high precision temperature measuring element, and is connected with a high performance 8-bit microcontroller. It communicates with the outside via ONE-WIRE.
AM2302 pin assignment:
1. VCC
2.SDA
3.NC
4.GND
Hi there,
It is digital sensor. We will check the package with product manager and update if it is wrong. thanks for pointing it out. thanks, 
Bill
Thanks a lot for your support.