PC interface planned?

Hi there!
I have received the DSO Quad two days ago and I have enjoyed it very much.
I’d like to ask you some questions…
The knobs aren’t practical: they are too small and I have difficulty to press them. Over that, to scan the various functions, you have to shift the knob left or right. Now, why didn’t you used a rotary knob, as many mobile phone used?
Another curiosity: is it planned/available any interfacing to a PC?..I 'd love having a graphical interface on a PC, maybe connected via USB.
Thanks a lot.
Cheers

cgi.ebay.com/New-DSO-2090-USB-PC … 1c1a6992e0

it is possible to translate the data to PC via USB, make it to be a virtual OSC. actully ,some friends have been doing this work with DSO nano viewtopic.php?f=12&t=1772

Yes while this is the case for the Nano (to be found here viewtopic.php?f=12&t=1772&start=50 ) , until we have a file export format for the quad projects such as mine and reinderien’s wont work but they do serve as a good example of what could be achieved once an export format is designed and someone like benF writes the firmware to export it.

CHeers Pete.