I wonder if anyone can give me the part number for the JST power connector which mates with the onboard connector found on the Seeeduino. I think I actually need two numbers: one for the housing and one for the crimp pins. I am aware that this connector is available with pigtail wires from the Seeed Studio Depot.
Ok, I found the part numbers.
Housing: JST XHP-2, Digikey 455-2266-ND
Crimp pins: JST SXH-001T-P0.6, Digikey 455-1135-1-ND