Panelising again.

i really not understand
at page seeedstudio.com/blog/2011/11 … alization/
“It’s only available for sizes like ‘5 cm Max * 5cm Max’, ‘5 cm Max * 10cm Max’, ‘10 cm Max * 10cm Max’, ‘5 cm Max * 15cm Max’, and ‘10 cm Max * 15cm Max’”

but at page seeedstudio.com/depot/fusion … ?cPath=185
“For the service ‘5 cm Max * 5cm Max’, ‘5 cm Max * 10cm Max’, ‘10 cm Max * 10cm Max’, ‘5 cm Max * 15cm Max’, and ‘10 cm Max * 15cm Max’, you can panelize to save the cost, but you need to cut the board by yourself.”

so that is wrong?
can you cut boards or not, and that is Clarification to panelizing?

You can put two or more designs on the same board, but you have to cut them apart yourself.