Hello
A question regarding SenseCAP T1000, is it possible to connect two SenseCAP T1000 through P2P? This feature is useful in places where LoRaWAN gateway is not available. In this case, one of the modules plays the role of the transmitter and the other the role of the receiver, and the receiver can transfer the information received from the transmitter module to the mobile via Wi-Fi or Bluetooth.
This feature can be seen in some similar trackers available in the market such as RAK2171 TrackIt.
2 Likes