Over-Current protection on Motor Shield V2.0

Hi!
I think my Motor Shield V2.0 was exposed to an over-current situation. I get an operating voltage on 1 pair of the motor terminals, but not on the 2nd. The sales information indicates an over-current shutoff, but I can’t find anything about it in the reference material. I also notice there are replacement parts available. Is this protection a single-use feature (like a fuse), or is there a way to reset and reuse it? Thanks.

Hi,

Can you please use the attached library and let us know the results.

Thanks and Regards
MotorDriver.zip (4.26 KB)

I reloaded the sketch with the new library and still get no output from the motor channels. The LEDs are indicating that the channels are changing polarity, but there is no current being output.

Suggestions?