Open parts library, 32768Khz crystal missing

Hi

While you have RTC IC DS1307ZN it requires 32768Khz crystal, which essential for this IC operation and not available in open parts library.
Is it possible to add it there?

Hey @denys2,

Thanks for the suggestion! I will pass your suggestion to our R&D team. They are collecting the suggestion to OPL and plan for the update. Your suggestion will be very helpful!.

Leslie Liao

A 12MHz crystal would also be nice for V-USB atmega328 projects. If I prototype with USnooBie, it would be nice if I could keep using the same setup and do not need to switch to 16MHz and waste precious space with NOPs for timing adjustments in the V-USB code.

Thanks and regards,
Ivo

They are collecting the suggestion to OPL and plan for the update. Your suggestion will be very helpful!.