Hi,
I just bought the v2.1 version of the OLED 1.12" display. I’m a bit confused about its specs and the provided Arduino library.
According to the Seeed product wiki the v2.1 board has a SH1107G driver chip and should support:
- 128x128 pixels
- grayscale, 16 shades
- horizontal scrolling.
It also tells me to download the this OLED_Display_96x96 Arduino library. Here it starts getting confusing because the included examples (e.g /examples/OLED_SH1107G_v2/OLED_PrintNumbers/OLED_PrintNumbers.ino) say:
The new OLED module drive IC has two version,
1. SH1107G (Note: SH1107G does not support scroll, gray display)
2. SSD1327
So my question is: how do I get it working as advertised?
I’m using it with an Arduino MKR WiFi 1010 + MKR Connector Carrier.
Thanks,
Walter