Shaeto
                
              
                
              
                  
                  
              1
              
             
            
              Hi,
finally i unsealed box and tried to run this OLED but it does not work, i used “working” sketch from the OLED wiki page.
hardware is USB connected Arduino Nano (328P)
Mb OLED is broken ? I didn’t drop it.
Thanks!
P.S. OLED is absolutely dark when powered on, do i need to use pull-up resistors ?
             
            
              
              
              
            
           
          
            
            
              Is it a Electronic brick - OLED 96x16 Display?
Please try for the below test sketch.
#include <Wire.h>
#define OLED_address  0x3c
unsigned char fill_OLED=0x55;
unsigned char fill_string1[]=“SeeedStudio”;
unsigned char fill_string2[]=" OLED 96*16";
unsigned char fill_string3[]="@@@@@@@@@@@@";
extern unsigned char myFont[][8]; //PROGMEM
//==================================
void print_a_char(unsigned char ascii=0)
{
unsigned char i=0;
for(i=0;i<8;i++)
{
SendChar(myFont[ascii-0x20][i]);
}
}
//==================================
void setup()
{
Wire.begin();
init_OLED();
delay(10);
clear_display();
delay(500);
}
//========================
void loop()
{
int i=0;
display_test();
delay(100);
clear_display();
delay(50);
for(i=0;i<2;i++)
{
setXY(i,0);
sendStr(fill_string3);
}
while(1)
{
sendcommand(0xa6);
delay(1000);
sendcommand(0xa7);
delay(1000);
}
}
//=======================
void sendcommand(unsigned char state)
{
Wire.beginTransmission(OLED_address); //
Wire.send(0x80);//command mode
Wire.send(state);
Wire.endTransmission();    // stop transmitting
}
//==================================
void display_test(void)
{
unsigned char i,k;
//  unsigned char Byte=0;
//for(k=0;k<2;k++)
{	
setXY(0,0);
for(i=0;i<96;i++)
{
//      Byte=myFont[i>>3][i&0x07];
//SendChar(Byte);
SendChar(0xff);
delay(20);
}
setXY(1,0);
for(i=0;i<96;i++)
{
//      Byte=myFont[i>>3][i&0x07];
//SendChar(Byte);
SendChar(0xff);
delay(20);
}
}
}
//==================================
void clear_display(void)
{
unsigned char i,k;
for(k=0;k<2;k++)
{	
setXY(k,0);
for(i=0;i<128;i++)//clear all COL
{
SendChar(0);
delay(10);
}
}
}
//===================================
void SendChar(unsigned char data)
{
Wire.beginTransmission(OLED_address); //
Wire.send(0x40);//data mode
Wire.send(data);
Wire.endTransmission();    // stop transmitting
}
//===================================
void setXY(unsigned char line,unsigned char row)
{
unsigned char realrow=row;
sendcommand(0xb1+line);
sendcommand(0x00 +(8realrow&0x0f));
sendcommand(0x10 +((8realrow>>4)&0x07));
/*
sendcommand(0xb1+line);
sendcommand(0x00+((8realrow-1)&0x0f));
sendcommand(0x10+(( (8realrow-1)>>4)&0x07));
*/
}
//==================================
void sendStr(unsigned char *string)
{
unsigned char i=0;
//setXY(0,0);
while(*string)
{
for(i=0;i<8;i++)
{
SendChar(myFont[*string-0x20][i]);
delay(10);
}
*string++;
}
}
//=================================
void init_OLED(void)
{
sendcommand(0xae);		//display off
sendcommand(0xa1);		//seg re-map 127->0
sendcommand(0xaf);		//display on
//  sendcommand(0xa6);
delay(10);
}