ODYSSEY - X86J4125800 CPU Temp

I have a ODYSSEY - X86J4125800 and its working very well.
I would like to know what the normal CPU temperature range should be; my CPU is running as follows:-

50C with average 10% load on each core
54C with average 50% load on each core
60C with average 90% load on each core

Are these acceptable or should I be looking at additional cooling?

REgards

Glenn Holt
G8NOF

You can refer to the product data manual. There should be the content you need in Appendix A.

I think the CPU can run all the time at 60℃.