I need to know the maximum output current rating of the 5V pins of ODYSSEY - X86J4125 V2, I wasn’t able to find any information regarding the absolute maximum current ratings of the power pins on the pin headers of RP2040 as well as the Raspberry Pi pinout pins.
Sorry I’m late. All the 5V and 3.3V pins in the 28-pin and 40-pin headers have a max current of 1A.
Hi,
The ODYSSEY - X86J4125 V2’s 5V pins typically support up to 1.5A of current per pin. However, for precise details on maximum current ratings, especially for specific pin headers, I recommend checking the official technical documentation or datasheet of the board.
For RP2040 and Raspberry Pi pinout pins, the general maximum current rating is around 50mA per GPIO pin, but it’s best to consult the respective datasheets for exact figures.
Hope this helps!