Before I was using Quectel EM06-E and it has been working fine. Had to switch to the Quectel EM060K-GL and it seems to not work at all. When plugged in, I am unable to boot to the SSD that hosts my OS. In the bio menu, the ssd is not detectable. Is there any solution to this?
According to its official product page:
EM060K series are compatible with EM06 series.
Cellular modules can draw a significant amount of power, especially during startup. Ensure your power supply can handle the total current draw of both the Quectel module and SSD. If the module is draining power, it may affect SSD detection. Try to use a different USB or PCIe slot for the EM060K-GL.