ODYSSEY - X86J4105864 operating temperature range

Hello,
I would like to ask what is the temperature range of ODYSSEY - X86J4105864? Thank you

Hi @vergil
The working environment temperature of this board is best controlled between 0°c and 75°c.

Thank you. Can we expect some performance drops reaching the upper temperature limit?

Yes, as the temperature rises, the CPU will run less frequently.

Thank you, do you have some exact or at least approximate temperature until which the performance will not be affected and the CPU will run at full performance?
Can you also let me know about the lower temperature limit? You’ve mentioned 0°C, but does that apply to a cold start, or can we run the device in e.g. -10°C if it hit the negative temperatures already running?
Many thanks again for your answers.

J4105 work as full performance at 0-45℃ ambient temperature if the fan embedded. Intel mentions that this CPU operating rang is above 0℃. Your are totally right if the board already runing then the temperature drop to -10℃, the board will be working as before.

Thanks for the answer.