ODYSSEY X86J4105 w/ eMMC does not have Windows pre installed

Need help. The ODYSSEY X86J4105 w/ eMMC doesn’t have a pre installed version of windows. Went into bios to ensure that everything was properly enabled and still only boots to Shell. Any help? Thanks!

you can download at Microsoft. Windows ISO

That was going to be my plan because frankly, after extensive research, this boards does not have an onboard eMMC. It’s the $188 version, but because it took them 4 months to deliver it to me I forgot which one I bought and the box, regardless, literally says “eMMC Version Pre-Installed: Windows 10 Enterprise”. To me, that says that I bought the higher end model. Seeed needs to get on the ball w/ what packaging they use.

So next phase is to figure out how to put a OS bootable drive onto this thing. Do I do it from USB, SATA or M2? I have a free Samsung USB 3.1 & 320GB Samsung SATA 3Gbps drive. Any recommendations on which drive I can use to leverage as the bootable drive so that all I have to do is turn it on and start working? Regardless of OS

burn iso to usb storage, boot usb to install to the sata for the system. As you have the sata drive might as well give that a try.

FYI: all current data on drive will be over written.

Worked like a champ! Thank you sir!

Happy to help. …