ODYSSEY-X86J4105 not booting after bios reset

ODYSSEY-X86J4105
BIOS VERSION SD-BS-CJ41G-M-101-K X64

I have reset the above system Bios and since then I cant boot into Debian OS
Pressing F7 booting menu only shows EFI. System will boot into EFI shell and loop.

I can’t figure out why on hearth this is a issue, I know I didn’t update Bios to the latest version but either???

Could someone more knowledgeable than me shine some light on this issue please.

Thank you in advance

Yes, pls update the latest firmware, BIOS and EC.

Thanks Bruce that worked like a charm

I have the same problem. How did you update the BIOS?

Hi mate,

It’s pretty simple, just foloow the instruction here https://wiki.seeedstudio.com/ODYSSEY-X86J4105-Updating-Firmware/