I was wondering about how much current I can draw from 5 volt power pins from Arduino and Raspberry Pi compatible pins. I remember reading that Arduino was able to provide about 500 mA from the 5v pin at maximum and Raspberry Pi was able to provide up to 1A. However, I am not sure what Odyssey can provide.
Maybe there is some documentation of X86J4105 that I don’t know about?
Hi @k-Knight
The maximum current of Raspberry Pi and Arduino Pin both could be provided up to 1A.
Thank you very much, I just wanted to make sure.
Since for what I am planning to do i needed 500mA in peak moments.
If I am not being too annoying can I ask you whether this number was discovered experimentally or is there some spec I can read ?
Hi @k-Knight
These data are from Intel Shared documents.