ODYSSEY - X86J4105 dual usb c displays?

Will it allow for dual usb c displays?
Eg. Using both Usb 3.1 ports.

Best regards
Hans

Hi @Kepha

Do you mean can you use type C for power and display together? if so the answer is yes! You can use 1 cable to power and display (if you have a monitor that supports that).

You can check here for reference.

Yes.
Do the board the support dual displays? Over usb 3.1?
With equal image on both (they show the same area for my use.)

Best regards
Hans

X86 only has one USB TYPEC port. It does support dual display (HDMI and TYPEC).

Best Regards
Anson