ODYSSEY X86J4105 - Aux Connector

Can please someone confirm if the Aux connector is a combined audio and mic and if so if it is TRS or TRRS?

Thanks

@milasx Yes, It’s a combined audio and mic. But the headset is divided into Apple headset and Android headset. Ours is an Android headset hole.

Could you confirm the pin type, I am having issues getting the MIC working, See this image, which one is the wiring of the Odyssey?

Thanks

First picture is right.

Thank you.
Looks like that when I use a TRRS headphone & mic the right audio channel and the mic do not work.
Instead when using a TRS headphone (no mic) both audio channel works.
Can you please confirm if the mic can be fixed?

Thanks

@Bruce.Qin support have now told me that the Odyssey only works with TRS and not TRRS which I find very strange; Can you please confirm if the Odyssey aux connector is meant to have a mic functionality as advertised in the spec?

OK - I now know that the problem is due to the case that does not allow the jack to go fully in because the hole is not big enough. Without the side the panel the mic works.

@Bruce.Qin: can you please provide a new side panel with a larger hole?

Support TRRS and CTIA standard.

:joy:Pls contact tech support email [email protected]. Sorry for the inconvenience.

Support said that hat you will do a new side panel. Hopefully it will not take long.