Odyssey X86 - Alternative fan

Hello All,

There are quite a few different threads on an issues with Odyssey’s fan.
In my case fan is working (from time to time) but it’s quite loud… hence I would like to replace it with higher quality fan.

I don’t want want to modify original case so I need to find another fan which fits current heatsink.

Has anyone found fitting fan?
Or do you have any idea how to mount regular square fan into the odysseys heatsink?

Cheers,
VM

I’m using a 90mm computer fan to cool mine with the help of a case I downloaded and modified from thingiverse, it seems to work so far without any problems… My x86 didn’t come with a fan, so I’ve had to be creative and use the 5 volt raspberry pi pins and a step up converter, but I wouldn’t be surprised if you could modify the fan’s wires to work with a normal fan’s