ODYSSEY – STM32MP157C setup for program and debug with CubeProgrammer and CubeIde

Hy, I want to program the ODYSSEY – STM32MP157C using STM32CubeProgrammer and debug it using STM32CubeIde, what is the setup for these connections?
I’ve tried USB connection on CubeProgrammer using J2 but the board is not recognized, and I also tried uart connection (always using J2) baudrate 9600 Parity–>none but it tells me “Activating device: KO. Verify boot mode configuration”

I’ve tried also using the debug serial port but again the same error, please let me know the setup for these connections.

And also CubeMx actually can produce the DTS files, there’s a way to choose ODYSSEY – STM32MP157C board in it?

Thanks,
Antonio

Please refer to Wiki usage.It is still very different from the official DEVELOPMENT board of ST.